AXIS#.MOTOR.TEMPWARN

Description

This parameter is used to configure the motor temperature warning level as a resistance threshold of the motor PTC.

A zero value prevents any warning from being created.

Context

For more information see Motor and Motor Temperature View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Range

0 to 2,000,000,000 Ω

Default Value

0 Ω = switched off

Data Type

Integer

See Also

AXIS#.MOTOR.TEMP
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
AXIS1.MOTOR.TEMPWARN

500bh

1eh

Unsigned32

-

-

Read/Write

No

AXIS2.MOTOR.TEMPWARN

510bh

1eh

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.TEMPWARN

6219

184B

Unsigned32

Read/Write

-

AXIS2.MOTOR.TEMPWARN

71755

1184

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TEMPWARN

6219

Unsigned32

Read/Write

-